Hi Expert,
How do I define the LP8557 Iout for per channel? Does it Imax/PWM resolution? Thanks!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Jerry,
I am not sure if I fully understand the question. You can control LP8557 brightness using either a PWM input and/or programming the brightness register. The mode selection is BRTMODE in register 0x10. The max current can either be set by using a resister or programming the MAXCURR in register 0x10. Please refer to section 8.6 in datasheet for more detail.
All these controls are for all 6 Channels, there is per channel control on brightness. However, you can turn ON/OFF each channel by programming LEDEN register (0x14). This setting should be done before you turn on the LED.
Regards
H L