The UCC28513 datasheet selects the R2 sense resistor by setting Vdynamic to 1 V. Is there a min and max range that Vdynamic can use for proper operation of the converter? If I increase the max current by adjusting the ratio of R7 and R14 to the PKLMT pin without changing R2, Vdynamic increases. Is there a max voltage across R2 which should not be exceeded? What happens when the max is exceeded?