Dear employees,
I recently ordered two LM2700 Step-Up PWM DC/DC Converter. One of them should power a Microcontroller-Board with 8V and 140 mA. The other one was considered to power a cooling device with 5V and 1.3A. Both set-ups (8V and 5V Output-Voltage) were given in the Application Information section of the data sheet at page 11 (8V) and page 12 (5V).The range of the input voltage that I adjust on the Vin-pin of each Step-Up-Converter lies between the recommended values of 2.5V and 4.2V. Also my power sources are able to provide enough current to power my devices.
And now to my problem: As long as I don't connect any load (Micorcontroller-Board or cooling device) to those settings described above, the Output-Voltage is stable at 8V and 5V. But as soon as I connect those loads the Output Voltage drops. Even with the highest Input Voltage recommended at 4.2V, I only receive 7.4V at the 8V Output setting and 2.95V at the 5V Output setting.
I also tried to replace the devices by using resistors that were scaled to pull the same amount of amps as the devices. But this set-up still gave me the same results.
My question now is if the voltage drop is considered to be the usual behavior of the LM2700 or did I make any mistakes in my set-up?
Thank you very much for your efforts.
Best regards
Simon Horneber