Hi!
I have the circuit of the image mounted on PCB but using tps28226(And using 6.5 V as a source for the driver), there are no problems with the devices or continuity. The driver is working fine when is not connected to the rest of the circuit, but when i connect the mosfets, the drivers stops working fine and in some point it gets hot and a short circuit appears between LGATE and GND.
I've been trying everything, but there are no problems with other devices or the PCB
What can be happening?