This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ24030EVM / BQ24031EVM differences

Other Parts Discussed in Thread: BQ24030EVM, BQ24030, BQ24031

As I am interested in buying a dual input battery charger demo, I find the BQ24030EVM and BQ24031EVM demo boards. Does anybody know if there is any technical differences between the two demoboards and why the BQ24030EVM is 150€ and the BQ24031EVM 44€ since both components have almost the same caracteristics. Thanks in advance for replying

Alphonsine

  • Alphonsine,

    The only difference between the bq24030EVM and the bq24031EVM is the IC populated on the board. 

    The bq24030 has a regulation voltage of 4.2V and the bq24031 regulates to 4.1V.  There are no other differences.

    Thank you for pointing out the difference in the pricing for these two EVMs.  I will get that resolved.

    Regards,

    Dick