Hello,
I need to design SMPS with the following spec to work as power supply for 3 phase inverter. (IGBT and uC power supply)
Input 175v to 450v AC,50Hz
Multi Output: 15v,0.3A x 4 nos. all isolated. 10% regulation ok
7v, 0.5 x 2 nos. all isolated. I will use Series regulator here. I will use one of 7v as opto input and load remains constant. So cross regulation wont be be a problem, I hope.
I have opted to use UCC28740D or TL2844D.
Kind request to clarify my below doubts
1) Do you suggest any other IC or my selection is ok ?
2) If i use UCC28740D, can I use voltage divider to connect HV pin to limit to 700v ? I do not want to complicate with HV transistor based series regulator
3) Any application note with simple part count for the same ?
4) Can the freewheeling diode be rated to block ~200v ?
5) Any suggestion tool for transformer design. As of now I use PI Expert !
Kind Regards,
Balaji R