The stated max value for this test on page 5 of the datasheet is 0.5v. When I do this test I get about 0.8v. Can you tell me the proper way to perform this test to get a typical value? The data sheet says that if an application requires the TPS54550 to be disabled then use open drain or open collector output logic to interface with the SSENA pin. Can you tell me why this is necessary? If I just use a regular voltage source will this cause the disable low level input voltage to be affected?
Thanks