This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
As we all know that UC2844 is a current mode PWM controller, pin3 is used for current sense and circuit protection. Quote on datasheet:
"An external series resistor, RCS, senses the current and converts this current into a voltage that becomes the
input to the ISENSE pin. The ISENSE pin is the noninverting input to the PWM comparator. The ISENSE input is
compared to a signal proportional to the error amplifier output voltage"
Based on diagram below:
Based on my understanding, the feedback of output voltage and reference voltage make up the voltage, comparing with Visense, if Visense is larger, the output of IC will be low level, which means MOSFET will not work.
Then in the circumstance that output voltage has hit the set voltage, which means error of voltage is 0, dose it mean the limitation of Visense is 0V at that moment?
And another question is, how this IC limit the power of circuit?
Thank you all