Hi team,
Please help to confirm the characteristics of TPS61163A. Thanks.
1. Can TPS61163A support minimum 0.5% PWM Duty Application?
2. What is the steady switching Ipeak current and max boost switch current of TPS61163A?
Thanks
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi team,
Please help to confirm the characteristics of TPS61163A. Thanks.
1. Can TPS61163A support minimum 0.5% PWM Duty Application?
2. What is the steady switching Ipeak current and max boost switch current of TPS61163A?
Thanks
Hi,
The TPS61163A can support 0.5% PWM Duty Cycle.
The max boost switch current (current limit protection) is typically 1.5mA. It can be as low as 1A and as high as 2A (please see "PROTECTION" section in datasheet Electrical Characteristics table).
The steady switching peak current depends on a number of factors: VIN, VOUT, inductor value, boost frequency, efficiency (please refer to datasheet section 9.2.2 for detailed description and calculations).
Regards,
Angelos Tsiros