Hi,
About the interrupt of the LP8501
In the STATUS / INTERRUPT register ENGx_INT
When BIT is set, it is output from the INT terminal.
Which of the following conditions (1) and (2) is correct?
(1) When ENG1, ENG2 and ENG3 are all set, the INT terminal is output.
(2) If any one of ENG 1, ENG 2, and ENG 3 is set, the INT terminal is output.
Best Regards,