I bought a LMZ31710EVM but it is not working.
I linked 12V DC to the PVIN and PGND, select the 5v and 1MHz, also linked VIN and PVIN together. But the out put is only 2V.
Do I need to connect PGND and AGND together?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
I bought a LMZ31710EVM but it is not working.
I linked 12V DC to the PVIN and PGND, select the 5v and 1MHz, also linked VIN and PVIN together. But the out put is only 2V.
Do I need to connect PGND and AGND together?
Hi Bin,
PGND and AGND is shorted in module, you don't need to connect it on board. we have LMZ31710 user guide on TI website, you can check it with the board on your hand. pls contact local TI office for more support.
B R
Andy Chen
Do you mean that AGND and PGND are shorted in the chip? or shorted on the board?
When I apply 12V on the board, there is 0.7V between AGND and PGND. And 166 oHm between them when I didn't apply the 12V.
I see a jumper R15 on the schematic but it is not soldered.
AGND & PGND are connected to one another internal to the device. R15 does not need to be populated.
Can you send a waveform of the VOUT and PH node?