This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
My customer used TI designs PMP7840.
He liked this TI designs.
Currently, He need to design next their product.
Condition is 24Vin, 48Vout and 0.65A.
But PMP7840 can not accept input 24V.
He wants to use LM5025.
Could you tell me where we change design of PMP7840 for accept input 24V, please?
Best regards,
Shimizu
Hi Shimizu-San,
1. Yes.
2. The difference between the two devices are summarized in the first paragraph of the description in the datasheet.
Just make sure to use the parameters of LM5025C when you make calculations.
Regards,
Wangxin
Hi Wangxin-san,
Thank you for last support.
I add questions about previous your answer about below.
>5. Retune the compensation network parameters of the error amp
>6. If CBC is desired, CS1 would need to be used while CS2 would need to be grounded. See page 13 of datasheet
Q1: About No.5.
Please see the attached file.
Which part of circuit did you show about "the compensation network parameters of the error amp"?
Could you show detail part at this circuit, plsease?
-> Is it C17 and R19?
Q2: Could you let me know the equation for calculation of the compensation network parameters of the error amp, please?
Q3: About No.6.
Please see the attached file.
What do R38 and R39 mean?
Q4: I think that R24 and C34 is filter. Is it correct?
Best regards,
Shimizu
Hi Shimizu-san,
Q1: C41, C42, R41.
Q2: No dedicated equations for loop compensation. Small signal modeling will be helpful. Normally, lab experimental tuning is needed with the frequency response analyzer.
Q3: T1 is the current sensing transformer. The current is sensed on the primary side and get reflected to the secondary side and converted to a voltage signal through R38. I am not sure about the purpose of R39.
Q4: I agree. But the corner frequency is high though, i.e., 1.59 MHz.
Regards,
Wangxin