Hi Team,
We are evaluating TPS61169EVM at the following conditions.
ILED of measurement result does not accord with the calculated value at low PWM duty.
Obviously, we doubt our measurement environment but please let me ask one more question.
I got advice from you about VFB (Please refer to the following E2E).
https://e2e.ti.com/support/power_management/led_driver/f/192/p/554429/2030636#2030636
Therefore, I understand that I can control ILED exactly at PWM duty 1% to 100%.
(I understand that ILED accuracy depend on VFB and RSET so it doesn’t depend on other parameters)
Is my understanding correct?
If no, could you please let us know if you have any concern?
According to our customer, they would like to control ILED from around 1mA to 30mA using PWM signal.
So, this is an extremely important point.
------------------
[Calculation]
ILED = (DUTY * VFB) / RSET = (0.01 * 204mV) / 6.75ohm ≒ 0.3mA
ILED = (DUTY * VFB) / RSET = (0.02 * 204mV) / 6.75ohm ≒ 0.6mA
ILED = (DUTY * VFB) / RSET = (0.03 * 204mV) / 6.75ohm ≒ 0.9mA
-----
[Measurement result]
ILED = 1.818mA at DUTY=0.01 , RSET=6.75ohm
ILED = 2.091mA at DUTY=0.02 , RSET=6.75ohm
ILED = 2.455mA at DUTY=0.03 , RSET=6.75ohm
-----
[EVM conditions]
-VL=8.4V
-VIN=3.15V
-ILED = around 1.818mA to 30mA (Measurement result)
-PWM 3.3V, 50kHz, 1% to 97%
-LED 7strings
-RSET= around 6.75ohm
Regards,
Kanemaru