Hi Team,
Our customer would like to use CCM mode at output current = around 0A to 1.5A.
We understand that we can use CCM mode at light load conditions if we increase inductor value.
So, we guess that the inductor value which is higher than several hundred is necessary.
(I understand that disadvantage is that "Load response" worsens.)
Therefore, we would like to know an upper limit level of the inductor value of each devices.
[Conditions]
VIN=8V to 42V
VOUT=5V (+/- 5%)
IOUT=0A to 1.5A
Fsw=420kHz
Synchronizes to External Clock function
[LM22680]
I confirmed simulation of LM22680(L=470uH and Cout=6.8uF) by WEBENCH.
Then, phase margin is 57.3deg(please refer to the attached file) so I understand that this device does stable operation.
Could you please let us know if you have any concern and a recommended upper limit level of the inductor value?
[LM25005]
I can’t find WEBENCH of LM25005.
Could you please let us know if you have any Calculation tool and a recommended upper limit level of the inductor value?
Regards,
Kanemaru