I have a pack model using the BQ20Z75-V180 and Panasonic UR18650A cells. Packs in previous builds would "wake" at around 50% RSOC. Panasonic is now shipping these cells to be compliant with the new transport requirement to be "less than 30% SOC" for air transport.
The cells in my most recent production lot measure around 20% SOC when discharged, however, when the pack "wakes up" it is showing 0% RSOC.
Is this because it does not like the OCV that it sees when it wakes up? If so, is there any way to change this?
Thanks,
Larry