Other Parts Discussed in Thread: TPS610981, TPS610982, TPS61021A
hello,
in a boost mode TPS61291 ic supply current of 1amp.when input is 2.4v and output is 3.3volt.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello,
No.
The switch current limit for the TPS61291 is 1A.
The application that you are asking about will require a solution that has a device with a higher switch current limit.
I would recommend looking at the TPS610981 or TPS610982.
What I would recommend is going to the product page for one of these devices and input your circuit requirements into the webench tool on the right side of the screen. This tool will allow you to simulate the operation of this part to test to see if it will work for your configuration.