This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
I'm using solar charger BQ24650 to charge LiFePO4 9Ahr, 12V battery at 14.2V, 2A max.
Since we connect to load directly to the battery terminal after the sense resistor, the system load when it's not charging is around 250mA in idle state.
This is higher than precharge 0.2A so when the battery is depleted to ~10.478V, with 575K/100K divider at VFB < VLOW of 1.55V, the pre-charge timer seems to expire after 30 minutes and the IC seems to go to FAULT condition.
We would have to remove the solar input and reconnect to reset.
Is there a way to disable the pre-charge so that even at 10.478V, it can fast charge the battery to supply enough current to the load?
Perhaps we could also toggle /CE (mppset) to reset the cycle once a day to avoid potential timer issue.
I can't find what the fast charge timer value is. If the load is drawing 250mA through the battery or through sense resistor, the fast charge might take longer time to complete since it detects Vbat=14.2 but I charge is still greater than 200mA.
-Khoi
we are using SI7288DP-T1-GE3 and diode similar to TI EVM design. I thought the Rsense is used for current limit 2A detection as well.
So what you say should be ok to connect load before Rsense. we will get small power loss over Rsense during normal operation but it should not draw from solar input over 3A.
Khoi
The solar panel is 17V, 2A peak (30W). Solar panel will limit the load current. However, in some case we have 17V DC source to power the unit instead of panel so it will be an issue as the DC source voltage won't drop.
Reading the Application Report SLUA376–June 2006 (http://www.ti.com/lit/an/slua376/slua376.pdf):I'm seeing similar behavior in Topology 1 issue 1, 2, 3.If we use Topology 2, Design considerations and potential issues:
1. The total current is only limited by the IC peak current protection and the thermal protection thresholds but not the charge current setting pin ISET1 (Rsense in our case) . The charge current does not drop when the system current load increases, as shown in Figure 9. This solution is not applicable if the system requires a high current.
Considering all the input options, I think our best way is still topology 1 and we need to put part of system to sleep to make sure it draws less than precharge. Also maybe we can reduce the precharge time as shown in appnote Application Report SLVA473–August 2011
Do you agree?
Khoi
Hi Khoi,
If there is no misunderstanding, your question is about the operation when solar panel cannot support system load(including charging and SYS loading), right?
Or could you please verify your question? Thank you!
Best regards,
Ann Lien
iIf we set r_sense to 0.01 and since the chip amd FET are sized for 2A, we don't want to exceed it with larger than 2A solar panel (18W) but we will gain 0.4A I_charge full range.
We don't expect the solar to power yhe load aince the battery in series with thr load will suplly larger than 2A current for motor.
Khoi
Hi Khoi,
If we use RSR=0.01, then the I_charge will be 4A. If FETs and output component are set for 2A, it couldn't meet the charge current requirement.
Does "Gain 0.4A full range" mean the charge current will be 2.4A in your case?
Best regards,
Ann Lien