This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
My customer usse BQ40Z50-R1 to desig battery pack.
They found the BQ40Z50-R1 already in ROM mode before any parameters update.
Is there any way cause BQ40Z50-R1 into ROM automatic?
Hi Arking,
Is this a 2S, 3S or 4S battery pack? Can you provide more details on the battery pack voltage?
It's possible for the enter "ROM mode" if the checksum stored doesn't match the checksum calculated after a reset. Do the following:
13.1.47 ManufacturerAccess() 0x0061 Lifetime Data Block 2 This command returns the Lifetime Data with the following format: AABBCCDDEEFFGGHH.
Value Description
AA No. of Shutdowns
BB No. of Partial Resets
CC No. of Full Resets
DD No. of WDT resets