Hello,
I'm using the TPS65185EVM as a reference design, and I just noticed that the capacitors
C7, C12, C13, C26
are not listed in the BOM. Can you confirm they are all 4.7µF 25V X6S 1206?
Thanks
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello,
I'm using the TPS65185EVM as a reference design, and I just noticed that the capacitors
C7, C12, C13, C26
are not listed in the BOM. Can you confirm they are all 4.7µF 25V X6S 1206?
Thanks
Hi Markus,
They are also 25V X6S 1206.
That cell within the BOM is not tall enough to show the first row of designators, but the QTY is still 9 and those are the only remaining 4.7uF caps.
Best Regards,
Rick S.