Dear,
I am using LM2621 on our product - Application: step up from 3.7V to 11V (Vout) with typical application - reference circuit.
But in the absolute maximum ratings table: BOOT pins - maximum: 10V. In typical application: BOOT pin is tied to VOut.
So with Vout = 11V. Is It OK ? If it is not - which configuration for Application with Vout = 11V. Thanks
Regards,
Tran Dinh Nguyen