Hello,
I'd like to ask for urgent help. I've tried FPWM Mode so far in order to get a constant switching frequency, however, am now seriously considering AUTO Mode, too, in order to significantly reduce operating supply current at light loads.
Questions
- Is it OK to dynamically switch between FPWM Mode and AUTO Mode while the LM53602-Q1 is operating?
- My idea is to use FPWM Mode at heavy loads for its constant switching frequency and to use AUTO Mode at light loads to reduce supply current. The system can roughly know the load status.
- If it's OK, how will the transient response caused by the mode change look like? Can overshoot/undershoot voltage level at the output be estimated?
Additional Questions
- How can the Max current that flows into the BIAS pin in FPWM Mode be estimated? I saw a higher current than the data sheet specs (47 µA (Typ), 78 µA (Max)).
- The same question as the above in AUTO Mode - how can the Max current into the BIAS pin be estimated?
Best regards,
Shinichi Yokota