Hello,
my custopmer is searching for a battery backup solution for a processor module. Normally the board is supplied by a power supply. In case of a power down the battery should switch over and power the system. The processor module needs 5V/1.5A. The battery is allowed to charge slowly.
Requirements:
- battery should buffer the module for 2hr
- battery: 2-cell = 7.2V, 2.9Ah.
- Vin can be 24V or 5V
- Quick charging is not needed
Regards, Holger