HI Sirs:
Our customer using TPS68470YFFR for CCM, schematic as below,
when they want to boot up world facing camera, CORE, VANA and S_RESETN are low level.
From datasheet 8.3.3.1,
" When SDA and SCL are routed to GPIO1 and GPIO2, the mode for these GPIOs must be
configured using their respective GPCTLxA registers as inputs with no pull-ups."
Is that means GPCTL1A and GPCTL2A bits[1:0] need to be reconfigured? if so, what's value should we use?
And is this related to this issue?