I'm looking to use the TLC5940 to drive a 9W 12V RGB LED. While 12V supply itself would not require the MOSFETs in this design, I would like to use them to offload heat.
The LED needs around 250 mA per color channel, too much for a single output.
Even with 3-4 outputs in parallel, the heat load on the TLC5940 will be too high. Forward voltages are 5.5V for red, 7V for green, and 8V for blue. My rough calculations puts this at up to 3.5W for the TLC5940 when used on its own.
Can I achieve good operation by connecting 3-4 outputs in parallel to a single N-MOSFET, to reduce the Vout while providing a higher current?
Or would I need to use one MOSFET per output?