Other Parts Discussed in Thread: USB2ANY
On startup of the SW, states I need an update of USB2ANY FW to version 2.6.5.3. It tries to do this, but fails by stating that the usb plug was unplugged, but it wasn't. I can recover with SDK firmware Loader and it fails repeatedly.
Am able to update the FW using the USB2ANY SDK Firmware Loader, but I only have USB2ANY_2_6_3_0.txt. Was able to find: USB2ANY_2_7_0_0.txt in terms of finding another fw file (which in itself was painful to find) but EVM wants/needs 2.6.5.3.
I have been able to use this USB2ANY hw with another dev kit (and i have 2 different USB2ANY) so I believe the hw is fine as works and only fails with the fw update.
This kit was mighty expensive to ship with supporting hw and sw in this state.
Any help would be appreciated.