Other Parts Discussed in Thread: TPS40140,
I'm looking for a solution to control the output voltage (or current by design as current source) as simple as possible and in a linear way. The output stage must be parallelized (50A maximum), so the stackability is important and TPS40140 or TPS40180 are ideal an a first view.
The idea was to use the TRK (40140) or SS pin (40180) to control the master via TRK and the slaves have to follow. But is this allowed, what happens after activating of internal fault circuits at 1.4V and after it, shutting down the TRK pin in a voltage range of 0...0.7V?
I have searched for it, but haven't got a result. I could try it out, but a theoretical approach is needed to be sure.
Thanks in advance...
Frank