Hello,
I am testing a product using the BQ27426, and I encountered a strange issue. The product has a 10000mAh battery, and the terminate voltage is set to 3.2V. The BQ27426 reports a SoC of around 50% with the battery at 3.8V. However, when a large current (4A) is drawn from the battery, the voltage drops due to resistive losses in the wiring to around 3.4V. The BQ27426 measures both the voltage and the current correctly, but starts decrementing the estimated remaining capacity (and SoC) very rapidly, much faster than a coulomb counter should. I guess this is related to the voltage drop, but it causes serious issues, since the SoC because pretty much useless. Is there anything I can do about this?
Thanks