Part Number: TLV431
Hi all,
I am trying to build a constant current sink using the TLV431 as a voltage reference and a NPN BJT (BC549C) on the output.
The circuit is shown below:
VG1 is the PWM signal (0-5V nominally), AM1 is used to monitor the current flowing from the 12V battery while VF1 were used to monitor the voltage across the base and the emitter of the bjt.
From the simulation it seems to work, and from bench testing it seems to work too.
However I am not sure if I forgot anything, especially regarding the OFF state phase, where the Vref pin voltage is not regulated. What do you think?
Thank you for your help and time,
Andrea C.