Other Parts Discussed in Thread: TLVH431, LMV431
hello everyone,
I use the following design from SLVA987A with a TLV431:
I have the following issue, this circuit work very well with TLVH431 but not TLV431.
When the Vref voltage is lower than the internal 1.24V reference, the cathode voltage is set to high level (~Vsup).
But when the Vref voltage is higher than the internal reference, the cathode voltage go to the low Vka voltage and increase rapidly with an unstable transition.
I measure the following oscillograme of cathode voltage when it was out of expected situation:
For my application, I want to detect under voltage on power supply. With the TLV431, I have a flag when the power supply voltage (Vin) is under a certain value. I have a second threshold when the power supply voltage is upper another value (It's not expected for under voltage detection).
However, my application works well with TLVH431 variant.
Where does this difference in operation come from?
Thank you in advance.