Tool/software: Linux
Hi,
I use in my reference hw tps65273V power regulator which is initially configured by resistors to select proper startup voltage. The issue I have with this chip is that seems like it does not determine startup voltage and sets VOUT_SEL reg properly so later when OS boots and driver is probed the driver sees the actual voltage selector and not the minimum supported that is 0.68V.
I cannot see anything in the datasheet to confirm this is the expected behaviour and I should explicitly update VOUT_SEL with an initial value (startup voltage) somewhere in a boot code. Also, cannot find any info if this chip has any circuit to determine start-up voltage.
Q: Should TPS65273V determine startup voltage by itself, so I can read out startup voltage from vout_sel reg?
FYI, I run Linux on my reference board.
/Waldek