This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ24195: dose SW support external MOSFET?

Part Number: BQ24195
Other Parts Discussed in Thread: BQ25895

Hi,

In my application, a 3A output current was required in battery boost mode, is there any way that I can achive it with BQ24195 chip?

  • Hello,

    You may be able to achieve this with two bq24195 chips in parallel, basically load sharing. But with a single chip, you cannot.

    You may also want to look at the bq25895 which has up to 3.1A OTG current limit.


    Regards,
    Joel H
  • Hello Joel,

    Thanks for your reply, it's really helps. bq25895 meets my requirements at all. one last question, compare with bq24195, bq25895 all ways need a external boost chip right? (in case for 5V/3A output)