This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM3488Q-Q1: LM3488's Various Characteristics

Part Number: LM3488Q-Q1
Other Parts Discussed in Thread: LM3488

Hi, team.

In selecting this IC, I would like to investigate the fluctuation rate of the feedback voltage under the following conditions, is it possible?

Condition: Switching frequency 100kHz

Vin = 24V (± 10% or ± 5%)

Operating ambient temperature -10℃~60℃

As for data, I would like if there is temperature characteristic and Vin characteristic of VFB.

Could you help us?

Best regards,

Masumi Sekiguchi