This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
hi,
I often see application where the voltage regulator is used as a constant current source to drive LED.
In my circuit below, if the MOS switch is always on, a constant 15mA flows through the LEDs.
If I use a PWM signal to switch the MOS switch so as to dim the LEDs, do you see any issue with LM1117 in the long run? Thanks.
Best Regards,
kpk