Other Parts Discussed in Thread: BQ27530-G1, , BQ24161, BQSTUDIO
In my current project, I am using the bq27530-G1 fuel gauge as well as the bq24161 battery charger. For evaluation, I am using the bq27530EVM which comes with both parts. In order to comply with the requirements given by the battery supplier's datasheet for the charging current, it shall not exceed 0.5C which translates to about 550 mA. The bq24161 provides the “Battery Termination/Fast Charge Current Register”, which allows defining the maximum value for the charging current, ICHRG[4:0].
In my application, the configuration of this register shall be done by the fuel gauge. Even though it’s possible to watch the status of the ICHRG[4:0] bits in bqStudio (image below), there is apparently no field in the fuel gauge’s flash settings (Reg 00 to Reg 07 in Charger Info) which allows to set their value. This means that the charging current programmed into the charger will depend only on the current calculated by the algorithm, as far as I understand. Is there any way to actually define a limit for the charging current with the bq27530 fuel gauge as host for the battery charger?