Other Parts Discussed in Thread: BQSTUDIO, BQEVSW, , BQ40Z50-R1
I have a battery pack from the first lot the vendor shipped to us, and one from the second lot (which were programmed with the wrong Chem ID). I reprogrammed both with the correct Chem ID and also with our “golden” parameter file with the following filter: all parameters were programmed (including calibration) except not the Ra Table. I assumed the default Ra Table was as good or better than what we have in our “golden” parameter file. After doing this, I expected the Static Chem DF Signatures to be identical, but lot 2 was C362 hex and lot 1 was 4362 hex. They’re close, which is suspicious, but not the same. Can TI shed some light on this? The only difference between the packs that I’m aware of is lot 1 has 2 thermistors where lot 2 only has 1. Thanks for any help on this mystery. I'm using BQ Studio 1.3.76 (the "test" version).