This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ25703A: bq25703A / Current Limit Setup after CHRG_OK goes HIGH

Part Number: BQ25703A


Hi,

Now I'm evaluating bq25703A EVM and then find the different behavior compared with description in datasheet. the section 8.3.2.2 describe that the input current limit set to default after CHRG_OK goes HIGH, but it looks like it may be set to default after CHRG_OK goes "LOW", not HIGH. Please see attached waveform and give your opinion.

[Test condition]

  • Use 2S battery
  • Load is 1.0A constant current
  • Charge current setting is 0mA

Best Regards,

Satoshi / Japan Disty