Hi everyone,
I have a (typical) circuit with TPS61221, 3V coin cell battery as input and a slide switch in series as you can see below in the schematic. The load current is 1~20mA in normal operation. I have noticed that sometimes when I turn the switch ON, the TPS61221 doesn't start and the output voltage is approximately 1.5V and the battery consumption is 200mA. I read some similar posts in forum so I added more input capacitors, but the problem remains. Why is this happening and how can be solved? Thank you in advance. I look forward to your response.