Other Parts Discussed in Thread: BQ24070
Hello,
I am testing the BQ24070EVM and am having trouble charging a deeply discharged battery. The battery is a 3.7V LiPoly which has a safety circuit that drops the output to 0V when the battery is below 3V. There is another thread on the forum about this: which never received an answer.
I followed the test procedure in the EVM manual and made the following observations:
1. With the battery plugged in and DC power supply off, VOUT is at 0.20V.
2. After supplying 5.25V to IN, VOUT at 0.20 V but all three LEDs were on, indicating that the system was in the pre-charge state.
3. After 5 minutes, VOUT still at 0.20 V and precharge LEDs still on.
4. I unplugged the discharged battery and power supply, and connected a charged battery. VOUT at 4.4V. Turned on power supply, STAT1 and PG LEDs on, VOUT at 4.4V.
5. I unplugged the charged battery and power supply, and connected the first battery again (its output now at 3V). Turned on power supply, STAT1 and PG LEDs on, VOUT at 4.4V.
6. Discharged the first battery fully again (output 0V), reconnected to EVM. VOUT at 0.20V. Removed the load, then replaced it (as suggested by the test procedure). Turned on power supply, STAT1 and PG LEDs on, VOUT at 4.4V.
Is there a way to "unlock" the battery for charging without disconnecting it or the load? Would adding a capacitor on DPPM to delay the short circuit help? The power management system will be enclosed inside a device so I would not be able to physically disconnect the battery/load when the battery becomes discharged.
Thanks!