Other Parts Discussed in Thread: TPS61098
HI,
I am checking the power save mode of TPS 61028.
For continuous mode and power save mode, the timing of the behavior of
these two modes is changed, what kind of conditions are there?
Is the output current lowered and the inductor current become discontinuous operation?
(specification)
VIN: 1 V to 3 V
VOUT: 2.8 V
IOUT: max 100 mA, the standby current is under consideration
Best Regards,