Hello guys,
One of our customers is considering using TPS54227. They have a few questions as the follows.
Q1. In TPS54227 case, the output of DCDC using the device is not connected to the device directly (Divided output voltage is connected to VFB. But it is not connected directly.) . What is the output voltage of TPS54227 limitted to 7V by?
Q2. If the output voltage is set to 7.5V or 8V, what is happend?
Your answers would be appreciated.
Best regards,
Kazuya Nakai.