This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
Customer want to use TPS259231 for their type-c application as the 5V VBUS current-limit switch. They need to support 3 type-c current limit (0.9A, 1.5A and 3A) by configuring 3 corresponding Rilim resistor value. From the datasheet, I found the minuimum current limit we can support is 1A, so we have a problem to support 0.9A. Do you have any idea to support this using TPS259231? Or you'll propose any other chip?
Thanks!
Antony