Other Parts Discussed in Thread: TPS720,
We currently use a TPS72010 and a TPS72012 to generate 1.0V and 1.2V outputs from a 1.5V supply. The BIAS-pin of the TPS720 is connected to 3.3V. While this generally works well and saves a lot of power compared to an LDO that is sourced from 3.3V, we have the problem that we can not control the sequence of the BIAS and VIN voltage sources. Since the TPS720 has the "VIN ≤ VBIAS under all conditions" requirement, we want to replace the device.
The LP5910 would fit nicely into the existing design, the TPS720 BIAS would connect to the LP5910 EN pin, which would be OK, all other pins match. The LP5910 would be sourced solely by the 1,5V rail, which would be within the Input Voltage Range.
But I'm unsure if the LP5910 would work with a fixed output of 1.2V when sourced with 1,5V. We would only use about 100mA.
Another problem is that the LP5910 seems to be listed in all the selection tables to be available with 1.2V fixed output, but there does not seem to be an according order option. How would I buy a LP5910 with 1.2V output?
Regards