This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
I have a strange problem that I am trying to overcome. The buck/boost switcher below converts a 12 volt rail to a 5 to 55 volt rail (output voltage is controlled by a micro controller via PWM to an optocoupler). The output rail powers two low frequency coils (125KHz) that are antennas for an RFID exciter. The load on the switcher is pulsy as the coils are OOK to produce a signal the receiving tags understand.
The design works and is currently in production, but what we are finding is that 5% to 10% of units exhibit a problem where the switcher gets stuck while ramping to set point. Usually the switcher gets stuck at an output voltage of about 3.3 to 3.5 volts. At the time the switcher gets stuck there is no load on the output. At the FB pin we can see that the control loop is trying to push the output higher, but the switcher is unresponsive.
Any ideas?
You are right. I neglected to answer that. Loading helps.
Any load below about 250 ohms helps. The switcher no longer gets stuck.
Thanks for the help.