This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
I built a circuit based on "Increasing Available Load Power in an LM2587 Boost Regulator" app note (its link is http://www.ti.com/lit/an/snva552/snva552.pdf). The difference is my input is around 24VDC, the output I want is 28VDC.
The circuit is working fine when there is no load at all! The output is 28VDC, and when switching the circuit ON/OFF, the circuit is working fine.
But when putting a load drawing current 1A, the input voltage drops to 3.5V insteading of 24V DC.
If I switched ON the circuit without load, then connected the 1A load afterwards, the circuit is working fine and the output is drawing 1A.
But if I switch OFF the circuit and then switched it ON (with the load connected), then the circuit failed to regulate. Any thoughts please?
Thanks in advance.
You may add an external soft start circuit to slow down the startup and hence the inrush current. The concept is presented in a TI app note at the following link: