This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS54521: TPS54521 S/C Output

Part Number: TPS54521

Hello
We have been using the TPS54521 for approx 5 years without problems. - (approx 40K pieces)
On one design we are see a very high rate on failure in that the device fails and the output goes S/C - approx 1.6ohm
This design is on a 3G GSM Modem - Vin = +12V - Vout = 3.7V at 2A (max) - normal operation <50mA)

We are using the same design as used on other products - Vin = +12V - Vout = +5V @ 4A max

Anyone else seen a similar problem or can help

Kind Regards
Paul H