This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM5118EVAL: LM5118EVL

Part Number: LM5118EVAL
Other Parts Discussed in Thread: LM5118

Hello All,

I bought the LM5118 evaluation board and now I am trying to get a (12 V at 1 A) output.

I connected a resistor load at the output and apply the voltage from 5 to 15V to the input.

The problem is with the input voltage below 10 V the EVB does not work ( I can hear some noise from the inductor !)

I am also sure my power supply can deliver above 5 Amp.

According to the datasheet of the evaluation board (page 4: Note that this design uses a current limit value to guarantee a full 3 A of output current at a minimum VIN of 5 V.) I should be able to get the output voltage 12v@1A when the input voltage is 5 volts , but by some reason it does not work.

Please kindly help me on this issue.

King Regards,

Ali