Other Parts Discussed in Thread: LM5118
Hello All,
I bought the LM5118 evaluation board and now I am trying to get a (12 V at 1 A) output.
I connected a resistor load at the output and apply the voltage from 5 to 15V to the input.
The problem is with the input voltage below 10 V the EVB does not work ( I can hear some noise from the inductor !)
I am also sure my power supply can deliver above 5 Amp.
According to the datasheet of the evaluation board (page 4: Note that this design uses a current limit value to guarantee a full 3 A of output current at a minimum VIN of 5 V.) I should be able to get the output voltage 12v@1A when the input voltage is 5 volts , but by some reason it does not work.
Please kindly help me on this issue.
King Regards,
Ali