Hi,
I have designed a PCB, derived from the TIDA-00669, for inductive charging functionality, battery management and the acquisition of physiological data using the analogue pins on the CC3220MODA.
A have a couple of questions:
[1] I would like to allow for a higher current flow (1500 mA), therefore I adjusted the Rs to ILIM to 9 (originally 200) Ohm and replaced the TPS63051 with the TPS63001. Have further changes to be made?
[2] If we want to cut off the power supply while charging and use the nCHG output on the BQ51050B to switch on / off a TPS63001 via the EN pin, do we have to use a pull-up-resistor or can we connect it directly?
[3] If we use the CC3220MODA on the same board with the power supply and the inductive charging what are the implications, especially with respect to ground planes?
Thank you very much,
Sebastian