This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS92512HV: Can TPS92512HV be used with TPS92661-Q1 or TPS92662-Q1?

Part Number: TPS92512HV
Other Parts Discussed in Thread: TPS92661-Q1, , TPS92662-Q1, LM3409, TPS92512, TPS92515, TPS92518, TPS92640

 Hello guys,

 One of my customer is wants to driver their LED with 2.5A using TPS92512HV. Also they want to use TPS92661-Q1 or 662-Q1 with the device.

 Is their any problem if TPS92512HV is used with TPS92661/662? If is there any concern, could you please give me your comment or advice?

 Your reply would be much appreciated.

 Best regards,

 Kazuya Nakai.

  • Hello guys,

    Could I ask an aditional question?

    Is LM3409 can be used with TPS92661-Q1 and TPS92662-Q1?

    Your reply would be appreciated.

    Best regards,
    Kazuya Nakai.
  • Hello Kazuya,

    The TPS92512 is a current mode control device. As a result it will not have the bandwidth to handle operation with the TPS92661/2 well.

    The LM3409 is hysteretic and designed specifically for such transients, it is very fast. Other options to use with the TPS92661/2 depending on the current you need would also be the TPS92515, TPS92640, or the TPS92518.

    The TPS92661 EVM uses the LM3409, it is the simplest solution for 2.5A.

    Regards,

    Clint

  • Hello Clint,

    Thank you very much for your prompt reply.

    I will recommend them to use LM3409/3409HV, TPS92640, and TPS92518(2ch output) because their requirement of LED driving current is 2.5A.

    Thank you again and best regards,
    Kazuya Nakai.