This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi!
I am working with LMR16006Y first time, and I need help in assessing the correctness of the layout of the circuit. All parts were calculated according datasheet with output current less than 100mA.
I think your schematic and layout are fair.
I have the following comments:
1. I would increase the value of C12/16 to 10uF
2. Need many more ground vias around C12/16, D4/5, C14/18 and the ground of the device. This will help to connect the grounds better.
3. Connect top of R3/6 closer to C12/16
4. Use as wide a trace as possible to pin2 ground.